News details

Vertiv Develops Energy-Efficient Cooling and Power Reference Architecture for the NVIDIA GB300 NVL72 Platform, Available as SimReady™ Assets in NVIDIA Omniverse Blueprint for AI Factory Design and Operations

Jun 11, 2025

New design demonstrates end-to-end energy-efficient cooling and power to support densities up to
142kW per rack

COLUMBUS, Ohio, June 11, 2025 /PRNewswire/ -- Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, announced its energy-efficient 142kW cooling and power reference architecture for the NVIDIA GB300 NVL72 platform. In addition to fully integrated end-to-end cooling and power strategies for this next generation platform, the reference architecture unlocks a new era of infrastructure design by shifting from traditional buildouts. Vertiv solutions are available as SimReady™ 3D assets in the NVIDIA Omniverse Blueprint for AI factory design and operations. The reference architecture can be customized for bespoke data center designs to dramatically reduce planning times and reduce risk during the buildout process.  

Vertiv works with NVIDIA and its data center roadmaps, to develop AI infrastructure strategies and deployment-ready designs that anticipate increased rack power densities. For example, Vertiv is collaborating with NVIDIA to support 800 VDC data center power infrastructure for 1 MW IT racks and beyond, with Vertiv solutions available starting in 2026.

"Building upon our strong collaboration with NVIDIA and a shared vision to advance AI infrastructure, Vertiv is proud to release our comprehensive reference design and SimReady™ 3D assets for the NVIDIA GB300 NVL72 platform," stated Scott Armul, executive vice president of global portfolio and business units at Vertiv. "Vertiv solutions allow customers to not only scale faster, but to optimize their AI-focused data centers digitally before a single physical module is built."

"By combining NVIDIA's advanced AI platforms with Vertiv's expertise in power and cooling infrastructure, we're enabling customers to deploy next-generation data centers that are more efficient, scalable, and ready for the most demanding AI workloads," said Dion Harris, senior director of HPC and AI Infrastructure at NVIDIA. "Together, we're helping organizations unlock new levels of performance and sustainability as they build the future of AI." 

The reference architecture for NVIDIA GB300 NVL72 is part of the Vertiv™ 360AI infrastructure platform, designed to help customers navigate integrated solutions for powering and cooling AI workloads and other high-performance computing applications.

Key benefits of Vertiv's reference architecture and SimReady™ 3D assets for the NVIDIA GB300 NVL72 design include:

  • Simulation to Deployment in One Path: Leveraging NVIDIA Omniverse technologies in the architecture bridges physical and digital infrastructure, enabling real-time system-level collaboration across IT, facilities, and engineering teams – allowing customers to test, optimize and validate the design before a single component is built.
  • Built for the Age of AI Reasoning: Supporting rack densities up to 142kW, the reference architecture for NVIDIA GB300 NVL72 defines the new benchmark for accelerated infrastructure — engineered for AI factories at scale.
  • Accelerated Performance, Scale, and Speed: Delivering 1.5x more AI performance, up to 50% faster on-site builds and in 30% less physical space, Vertiv's reference architecture for NVIDIA GB300 NVL72 enables customers to scale AI infrastructure with unprecedented agility and energy efficiency.
  • Thermal Flexibility Meets Efficiency Gains: Liquid cooling-ready, supporting both air- and hybrid- cooled configurations, achieves up to 70% better annual energy efficiency allowed by higher water temperatures.
  • Design, Deploy, Operate - Globally: Backed by 4,000+ Vertiv field service engineers globally, Vertiv's reference architecture for GB300 NVL72 brings unmatched scalability, serviceability, and supply chain reliability to global AI rollouts.

As global AI demand accelerates exponentially, Vertiv is constantly working to deliver critical energy-efficient cooling and power solutions, to enable AI-ready infrastructure to run the next generation of AI factories.

To learn more, visit Vertiv.com.

About Vertiv
Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers' vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today's data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-looking statements
This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv's filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT
Ruder Finn
E 
Vertiv@RuderFinn.com

Cision View original content to download multimedia:https://www.prnewswire.com/news-releases/vertiv-develops-energy-efficient-cooling-and-power-reference-architecture-for-the-nvidia-gb300-nvl72-platform-available-as-simready-assets-in-nvidia-omniverse-blueprint-for-ai-factory-design-and-operations-302478919.html

SOURCE Vertiv Holdings Co