News details

Vertiv Introduces Medium-Voltage Power System to Help AI Data Centers Connect to the Grid Faster and Free Indoor Space for Compute

Nov 12, 2026

The Vertiv™ PowerNexus MV UPS is an outdoor-rated, medium voltage system that combines medium voltage UPS, fault ride-through and AI power smoothing in a single platform.

Dedicated Medium Voltage Laboratory planned at the Global Large Power R&D and Customer Experience Center in Bologna, Italy, to accelerate next-generation AI power infrastructure.

COLUMBUS, Ohio, Nov. 11, 2026 /PRNewswire/ -- Vertiv Holdings Co. (NYSE: VRT), a global leader in critical digital infrastructure, today introduced the Vertiv™ PowerNexus MV UPS, a medium-voltage power solution designed to help colocation, neocloud and hyperscale data center operators accelerate utility interconnection, optimize site utilization, and support evolving grid requirements. Designed for outdoor deployment at the point of connection, the solution provides continuous power protection while helping preserve valuable indoor space for revenue-generating compute. It also delivers up to 98.5% peak operating efficiency and can help reduce reliance on diesel generators. Vertiv is engaging customers globally, with shipments expected to begin in mid-2027.

The Vertiv™ PowerNexus MV UPS is an outdoor-rated medium-voltage power system designed to provide power protection, support grid stability and help preserve valuable indoor data center space for compute. © Vertiv

"Data centers are facing new infrastructure challenges, including grid queues that can delay deployment and revenue generation, indoor space constraints that limit compute density, and evolving grid requirements that can challenge traditional infrastructure and architectural approaches," said Kyle Keeper, senior vice president of the power management business unit at Vertiv. "The Vertiv PowerNexus MV UPS is designed as a system-level response to those challenges, combining medium-voltage power protection, fault ride-through and AI power smoothing in an outdoor platform designed to operate with long-duration energy storage, helping operators to focus on deploying compute, not coordinating infrastructure."

Extending power protection and management closer to the utility connection point, the Vertiv PowerNexus MV UPS provides the following capabilities for AI data center operators:

  • Class 1 critical load protection. Designed to integrate with long-duration battery systems, the solution delivers Class 1 output voltage quality in accordance with IEC 62040-3, helping to protect critical loads during grid disturbances and upstream faults.
  • Indoor space savings. An outdoor-rated skid moves critical power infrastructure outside the data hall, helping preserve valuable indoor space for revenue-generating compute.
  • Fault ride-through and AI power smoothing. The solution is designed to support grid stability during fault conditions and absorb rapid AI load fluctuations before they reach the grid.
  • High operating efficiency. Line-interactive topology delivers up to 98.5% efficiency under peak conditions, helping reduce energy use and operating costs.
  • Reduced reliance on diesel generators. When integrated with long-duration battery systems, the solution can provide battery-backed operation of up to four hours, helping reduce reliance on diesel generators for long-duration backup.
  • Simplified deployment. A single-vendor skid architecture helps reduce coordination complexity across UPS, batteries and other powertrain components, helping streamline system deployment.
  • Faster, more confident system design. A Power Systems Computer Aided Design (PSCAD) model is available to help customers simulate system behavior, validate integration and assess power quality and dynamic interactions between the Vertiv™ PowerNexus MV UPS and the broader electrical grid before deployment.

Customer demonstrations validate Vertiv™ PowerNexus MV UPS performance

Vertiv recently hosted proof-of-concept demonstrations with QTS, SoftBank and Rosendin at its Global Power R&D and Customer Experience Center in Bologna, Italy. Testing across a range of steady-state and dynamic conditions demonstrated stable performance across 0–100% loads, Class 1 voltage accuracy during rapid load changes, and ride-through of significant voltage disturbances, including a 100% voltage sag for 150 milliseconds and 25% overvoltage for five seconds.

"Vertiv PowerNexus MV UPS demonstrated the performance and flexibility needed to support demanding AI data center applications," said Ryan Kuithe, senior vice president, facilities operations at QTS. "During proof-of-concept testing at Vertiv's Global Power R&D and Customer Experience Center, we validated the system's ability to maintain stable power through dynamic load changes and voltage disturbances."

Dedicated facility expands medium-voltage research, testing and customer engagement capabilities.

The recent interest in customer demonstrations highlighted the importance of Vertiv's dedicated Medium Voltage Laboratory at the Global Large Power R&D and Customer Experience Center in Bologna, Italy. Scheduled to become operational in 2027, the facility is designed to support research and development, full-voltage validation, customer demonstrations, service training, and system-level testing for medium-voltage power architectures, including MV UPS, MV to 800 VDC, and battery energy storage technologies. Customers worldwide can engage with Vertiv for demonstrations and system validation.

"By enabling full-voltage research and development, testing, customer demonstrations, and system-level validation, the facility will help customers evaluate new architectures with greater confidence as they plan the power systems required for AI-scale data centers, including 800 VDC," said Giovanni Zanei, vice president, large power conversion, Vertiv.

For more information about Vertiv's end-to-end power and thermal management solutions and expanding portfolio for AI and high-density workloads, visit Vertiv.com.

About Vertiv Holdings Co.

Vertiv Holdings Co. (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers' vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today's data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv's filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT
Vertiv@ruderfinn.com

 

Vertiv logo

Cision View original content to download multimedia:https://www.prnewswire.com/news-releases/vertiv-introduces-medium-voltage-power-system-to-help-ai-data-centers-connect-to-the-grid-faster-and-free-indoor-space-for-compute-302937910.html

SOURCE Vertiv Holdings Co